AXIS#.IL.COMMANGLE

Description

AXIS#.IL.COMMANGLE reports the commutation angle in degrees when the axis is enabled and generating current. The angle is determined based on the axis configuration:

  1. If AXIS#.OPMODE = 0 (torque mode) and AXIS#.IL.CMDMODE = 1 (UVW current command mode), the angle is calculated from the phase current commands when AXIS#.IL.SETCMD runs.

  2. If AXIS#.MOTOR.TYPE = 10 (surface permanent magnet with sensorless control) and AXIS#.OPMODE = 1 (velocity mode), the angle is calculated by the sensorless estimation algorithm.

  3. Otherwise, the angle is calculated by the feedback based commutation algorithm.

The commutation angle ranges from 0 to 360 deg over each motor electrical cycle. It reflects the commutation phase after AXIS#.MOTOR.PHASE has been accounted for. For any of the cases above, AXIS#.IL.COMMANGLE can be referenced to the U,V,W phases as follows:

  • AXIS#.IL.COMMANGLE = 0 deg when the current commands align with the U phase.

  • AXIS#.IL.COMMANGLE = 120 deg when the current commands align with the V phase.

  • AXIS#.IL.COMMANGLE = 240 deg when the current commands align with the W phase.

AXIS#.IL.COMMANGLE is set to 0 when the axis is disabled or when no current is being commanded.

Example

The following commands apply to case 1 above with the current command aligned between the U and V phases.

--> AXIS1.OPMODE 0
--> AXIS1.IL.CMDMODE 1
--> AXIS1.EN
--> AXIS1.IL.IUCMDU 1.0
--> AXIS1.IL.IVCMDU 1.0
--> AXIS1.IL.SETCMD
--> AXIS1.IL.COMMANGLE
60.000 [deg]

As a different example for case 3 above, the following WorkBench scope trace shows AXIS#.IL.COMMANGLE and FB#.MECHPOS while the motor is spinning at 300 rpm. For this setup, AXIS#.MOTOR.POLES = 6, so there are three commutation cycles for each mechanical revolution. Furthermore, AXIS#.IL.COMMANGLE leads FB#.MECHPOS by AXIS#.MOTOR.PHASE.

Versions

Action Version Notes
Implemented 02-07-04-000

General Information

Type

Read Only

Units

Degrees

Range

0 to 359.999

Default Value

N/A

Data Type

Float

See Also AXIS#.IL.CMD, AXIS#.IL.DCMD,AXIS#.IL.IUCMD, AXIS#.IL.IVCMD, AXIS#.IL.IWCMD

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COMMANGLE

500ah

24h

Unsigned32

-

1000:1

Read only

No

AXIS2.IL.COMMANGLE

510ah

24h

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5844

1

5844 (0x16d4)

AXIS1.IL.COMMANGLE

Unsigned32

Read Only

Yes

71380

2

5844 (0x16d4)

AXIS2.IL.COMMANGLE

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COMMANGLE

5844

Float

Read Only

-

Related Topics

Current Loop